2024-09-15 11:36 PM
Hello, I have a question: Is the NFC technology in the iPhone always active, even if the Wallet app is not in use? I mean, is it always emitting RF radiation to read/write?
Solved! Go to Solution.
2024-09-16 1:26 AM
Hello Jonamleonel,
I think you need to differentiate two scenarios:
About health effects: Due to the low frequency and the low power the consensus is that there is no risk here (even if it would be Constant Carrier.) Constant Carrier is typically avoided to save power.
BR, Ulysses
2024-09-15 11:57 PM
hi JonamLeonel,
Yes, NFC RF is always active on iPhone. Even if wallet App is not in use.
This allows to handle NFC background reading mode : the system scans for and reads NFC data without requiring users to scan tags using an app.
Hope it clarifies.
br,
2024-09-16 12:01 AM
Is it always emitting electromagnetic waves/RF ? Is it dangerous for people, many people uses its phones in the pants pockets
2024-09-16 1:21 AM
Well, you may need to ask Apple about the exact circumstances when and how NFC is active.
By “dangerous for people” do you mean a health risk or a risk to security or finances?
Regards
/Peter
2024-09-16 1:26 AM
Hello Jonamleonel,
I think you need to differentiate two scenarios:
About health effects: Due to the low frequency and the low power the consensus is that there is no risk here (even if it would be Constant Carrier.) Constant Carrier is typically avoided to save power.
BR, Ulysses
2024-09-16 1:29 AM
Safe for the body ?
2024-09-16 1:37 AM
When it comes to health, you should compare the radiation power emitted by smartphones with the different wireless bands. With GSM/LTE/5G we are talking about 2W transmission power, with NFC about milliwatts. If you're really worried about this, you should switch off your smartphone completely, shouldn't you?
2024-09-22 1:58 AM
Even if iPhone wallet app is deleting? The iPhone is emitting NFC radiation pulses ?
2024-09-23 5:11 AM
Hi,
don't know if you can even delete the wallet app. Even if so I would expect the background scanning service to be still operational.
Regards, Ulysses
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.