2020-08-16 11:37 AM
Hello ST team and Guys here.
We have a new project that requires us to measure the a position of a moving object with a range of 100 mm with an accuracy of +- 1 mm. I was wondering if by attaching a NFC tag to the object and a reader with a similar 100 mm read range, could we sample based on the time of flight or time stamps of tag read or tag count to achieve a +-1 mm of position accuracy. Can the algorithm based in NFC readers convert the tag time stamp or count to be used as position sensing with such high resolution.
Thanks and best
LK
Solved! Go to Solution.
2020-08-17 8:09 AM
Hi,
I cannot imagine such to work:
What you could do is to look at the RSSI value in the reader but that will be very rough and can only work if you can limit your system to one reader with exactly one tag.
It sounds a little bit like CoVid-19 tracing apps which are trying to use the Bluetooth for ranging. Also Bluetooth despite its 2.4GHz is here very in-accurate as it was not built for ranging and they rely on RSSI (Received Signal Strength Indicator) instead of time of flight.
Even protocols built for ranging like UWB (https://www.st.com/en/ecosystems/spark-sr1010-sr1020-ultra-wideband-radio-modules.html) are orders of magnitude away from a 1mm accuracy.
Regards, Ulysses
2020-08-17 8:09 AM
Hi,
I cannot imagine such to work:
What you could do is to look at the RSSI value in the reader but that will be very rough and can only work if you can limit your system to one reader with exactly one tag.
It sounds a little bit like CoVid-19 tracing apps which are trying to use the Bluetooth for ranging. Also Bluetooth despite its 2.4GHz is here very in-accurate as it was not built for ranging and they rely on RSSI (Received Signal Strength Indicator) instead of time of flight.
Even protocols built for ranging like UWB (https://www.st.com/en/ecosystems/spark-sr1010-sr1020-ultra-wideband-radio-modules.html) are orders of magnitude away from a 1mm accuracy.
Regards, Ulysses
2024-07-29 7:40 PM
Hi,
Can NFC tags be used between one another to create a grid?
For example, and without extreme accuracy, to understand that tag1 is located in back right corner of a small room. Tag2 is located in back left corner of same small room. And that tags 3-10 are in additional locations in the same room. Assuming that each tag is within 1-3 feet of one another.
Thanks,
jan
2024-07-30 12:22 AM
Hi,
I would suggest to create a new thread rather than posting on an already answer thread.
Thanks
Rgrds
BT
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.