2013-08-20 2:49 AM
Hello,
I'm using an RFID reader (Feig LRM1002) with 2 different version of the M24LRXX chip : - M24LR04E(ANT3-M24LR04E)
- M24LR16E(ANT1-M24LR16E and ANT2-M24LR16E)
A problem appear when I scan my tag :
When I send an ''Inventory'' command there are no problems, I can see both versions of the chip. The problem appear when I send a ''Read or Write Multiple Blocks'' command. With the M24LR16E I have an error message : ''No Transponder In Reader Field'' (it works well with the M24LR04E). I tried the ''Extended Adress Mode'' but it didn't change anything. Do you know what the problem could be ? For information I use the demo software provided by the reader manufacturer (Feig ISOStart). I took some screenshot : Thank you m24lr04e m24r04e 2-bytes m24lr16e devkit-m24lr-a m24lr-read-write-problem m24lr16e m24lr04e high-densitySolved! Go to Solution.
2013-08-22 11:55 PM
2013-08-21 2:31 AM
2013-08-22 12:22 AM
Ok, thank you. So I need to upgrade my reader firmware.
2013-08-22 1:12 AM
2013-08-22 2:41 AM
Ok, I already have some contacts with Feig. I'll contact them myself.
Thanks a lot for the infos2013-08-22 11:55 PM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.