2023-02-07 1:08 AM
hello,
I am working with ST25RU3993-HPEV baord. Getting all the list of inventoried tags in GUI (ST25RU3993 Reader Suite). I have gone through the ST25RU3993 SDK and tried to change the code to print the list of tags in uart. But iam unable to do so. Please help to identify the necessary chages required for printing the list of tags in uart.
Tahnk you
Solved! Go to Solution.
2023-02-17 1:10 AM
Hello Gk.3
The SDK provides smaple source code in C, C#, Python and Java to connected to an ST25RU3993 HPEV board via UART and start to scan for transponders.
When running inventory the ST25RU3993 board send cyclic information via UART to the host. The SDK provides callback functions were the application has access to the identified transponder data.
Could you provide more details what your issue is with "printing the list of tags in uart" ?
BR
Nick
2023-02-17 1:10 AM
Hello Gk.3
The SDK provides smaple source code in C, C#, Python and Java to connected to an ST25RU3993 HPEV board via UART and start to scan for transponders.
When running inventory the ST25RU3993 board send cyclic information via UART to the host. The SDK provides callback functions were the application has access to the identified transponder data.
Could you provide more details what your issue is with "printing the list of tags in uart" ?
BR
Nick
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.