2020-05-03 11:19 PM
Solved! Go to Solution.
2020-05-04 3:15 AM
Hi @VCecc.1 ,
Sorry I was wrong, I've read more carefully the datasheet of the ST25DV (https://www.st.com/content/st_com/en/products/nfc/st25-nfc-rfid-tags-readers/st25-dynamic-nfc-tags/st25dv-i2c-series-dynamic-nfc-tags/st25dv04k.html) and it is mentioned that registers can be read continuously but same behavior is not available for the write command (chap 4.3 p 17).
Hope this help you.
Regards.
2020-05-04 1:15 AM
Hi @VCecc.1 ,
This is strange, you should be able to write the 16 bytes in one command. I'm guessing that you are writing at address 0000h in the system area, so all 16 registers are accessible in write.
Do you have same problem writing in the user area?
Best Regards.
2020-05-04 1:53 AM
Hi Rene,
Yes, I set 0000h as start address then try to write 16 Bytes (from 0000h to 000Fh). It does not work. Session is open, in factif I write one byte at a time, I can customize/modify all 16 Bytes of Sys Config Area. If I try to do the same thing in User Area (same adresses but E2 bit = 0), it works, I write and read what I wrote.
Best Regards
2020-05-04 3:15 AM
Hi @VCecc.1 ,
Sorry I was wrong, I've read more carefully the datasheet of the ST25DV (https://www.st.com/content/st_com/en/products/nfc/st25-nfc-rfid-tags-readers/st25-dynamic-nfc-tags/st25dv-i2c-series-dynamic-nfc-tags/st25dv04k.html) and it is mentioned that registers can be read continuously but same behavior is not available for the write command (chap 4.3 p 17).
Hope this help you.
Regards.
2020-05-04 3:36 AM
Hi,
ok, I understand, thankyou for your precious info
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.