2020-05-11 3:26 AM
I2C is 400KHz, but I have same problem at other speed SCL.
I use ST25DV16K-I.
Solved! Go to Solution.
2020-06-04 2:45 AM
Hello,
Are you doing I2C read or I2C write ? I'm not sure I understood.
Read and write are different:
The programming time is ~5ms for 4 bytes. In your case, if you write 64bytes, the programming time will be 16*5ms=80ms (+/-5ms if you started on a non paged-aligned byte). So, in case of I2C write, it is normal that you cannot access the tag for ~80ms following the STOP.
In case of a read, followed by another i2c command, there is no delay required.
This is common behavior for EEPROM memories.
Does this correspond to your use case?
Best regards.
2020-06-02 12:21 AM
Hello Arnaud,
You should normally be able to start a new I2C read command immediately after the stop condition of the previous read command.
There may be some traffic on the I2C bus (to other slave devices ?) or traffic on RF interface ? If there is RF commands on going, I2C access is not acknowledged. Is there a RF reader with RF field ON present on the antenna when this happens ?
Best regards.
2020-06-04 12:55 AM
Hello,
thanks for response.
There are no traffic on I2C , only ST25DV16K-IN
Not traffic RF also, I just try to write or read memory, (as a classic memory...), without RF device close, I have also remove NFC antenna to be sure ! I have the same problem to read or write, I must wait about 100 ms between each read/write command .
Best regards,
Arnaud
2020-06-04 1:08 AM
The first command works always, and then, if I dont wait 100 ms, the device ST25DV16Kreturn NACK and STOP bit for the second command.
The command are the same to avoid error, I try to write 64 bytes.
Best Reagrds
Arnaud
2020-06-04 2:45 AM
Hello,
Are you doing I2C read or I2C write ? I'm not sure I understood.
Read and write are different:
The programming time is ~5ms for 4 bytes. In your case, if you write 64bytes, the programming time will be 16*5ms=80ms (+/-5ms if you started on a non paged-aligned byte). So, in case of I2C write, it is normal that you cannot access the tag for ~80ms following the STOP.
In case of a read, followed by another i2c command, there is no delay required.
This is common behavior for EEPROM memories.
Does this correspond to your use case?
Best regards.
2020-06-04 3:02 AM
Thanks you for your answer.
I have try I2C WRITE and I2C READ.
It seems my protocol to write and read is according with your epliaction. However, I understand now the problem for about 80 ms in WRITE.
it means that I probably have an error then in my protocol to READ...
I continue my investigations.
Best regards,
Arnaud
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.