2023-04-17 7:42 PM
Dear sir
It is being developed on the ST25ru3993 board. The external PA is not working, so I checked the power and it is 0V. The documentation says it should be 4.1V, but I want to know if I can make it work again.
Also, I want to know why the expansion PA is not powered.
If I configure another external PA circuit and use it, I wonder if I can operate it with that board.
If this is possible, I would like a circuit recommendation.
Thank you, sir
2023-06-12 2:16 AM
Dear esoft.1,
please could describe, which software are you using?
Is it an own software or do you use the ST software for controlling the board?
Thanks & best regards,
Marcel
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.