cancel
Showing results for 
Search instead for 
Did you mean: 

Capacitive wakeup and AAT with ST25R3911B RFAL

rabinniroula
Associate III

Hello, I couldn't find any examples with RFAL to use capacitive sensing and the usage of AAT. I'm using a single ended matched antenna. I tried using rfalAdjustRegulators(), it always gives a value of 3000. I also wanted capacitive sensing: the chip should wakeup and start polling only when a capacitance change is detected on the capacitive pads, otherwise it should be in low power mode (if possible). I've included the code I'm using. The function stateCB is being called frequently. I don't believe it's being triggered by capacitive sensing.

 

rfalAnalogConfigInitialize();
	PERFORM_WITH_LOG(err, rfalNfcInitialize());
	PERFORM_WITH_LOG(err, st25r3911SetAntennaMode(true, false));
	rfalWakeUpConfig wakeupConf = {.period = RFAL_WUM_PERIOD_100MS,
																 .irqTout = false,
																 .refWU =
																		 {
																				 .enabled = true,
																				 .refDelay = RFAL_WUM_PERIOD_100MS,
																		 },
																 .indAmp =
																		 {
																				 .enabled = false,
																		 },
																 .indPha =
																		 {
																				 .enabled = false,
																		 },
																 .cap = {.enabled = true,
																				 .delta = 3,
																				 .reference = RFAL_WUM_REFERENCE_AUTO,
																				 .autoAvg = true,
																				 .aaInclMeas = true,
																				 .aaWeight = RFAL_WUM_AA_WEIGHT_8}};

	rfalNfcDiscoverParam discParam = {.compMode = RFAL_COMPLIANCE_MODE_NFC,
																		.techs2Find = RFAL_NFC_POLL_TECH_A,
																		.techs2Bail = 0,
																		.totalDuration = 0U,
																		.devLimit = MAX_DEVICES,
																		.maxBR = RFAL_BR_106,
																		.GBLen = sizeof(GB),
																		.p2pNfcaPrio = false,
																		.isoDepFS = RFAL_ISODEP_FSXI_512,
																		.nfcDepLR = RFAL_NFCDEP_LR_254,
																		.notifyCb = stateCB,
																		.wakeupEnabled = true,
																		.wakeupConfigDefault = false,
																		.wakeupConfig = wakeupConf,
																		.wakeupPollBefore = true,
																		.wakeupNPolls = 1};
	memcpy(discParam.nfcid3, NFCID3, sizeof(NFCID3));
	memcpy(discParam.GB, GB, sizeof(GB));
	err = rfalNfcDiscover(&discParam);
	platformLog("Error in discover: %d\n", err);
for (;;)
{
  rfalNfcWorker();
  delay(10);
}

 

 

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
rabinniroula
Associate III

I performed refWU.enabled = false and it worked. The AAT was working from the begining.

View solution in original post

2 REPLIES 2
rabinniroula
Associate III

I performed refWU.enabled = false and it worked. The AAT was working from the begining.

Hi,

in this case the module should have told you such as it should return an error:

    if( ...
        ((gRFAL.wum.cfg.refWU.enabled) && ((gRFAL.wum.cfg.cap.enabled) || 
         ...  )
    {
        return RFAL_ERR_PARAM;
    }

I presume your request is resolved?

BR, Ulysses

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.