2017-02-23 2:49 AM
We are using the NFC03A1 board with Nucleo F103RB.
In the function :
int8_t PCD_ProtocolSelect(const uint8_t Length,const uint8_t Protocol,const uint8_t *Parameters,uint8_t *pResponse)
There is a buffer DataToSend[SELECT_BUFFER_SIZE] where SELECT_BUFFER_SIZE is 6.
Then we fit the buffer with datas depending on the Lenght argument... until '3 + Length - 1'
In the function : ISO14443A_ConfigFDTforAnticollision(), we can read :
if( IcVers >= QJE)
NbParam = 6; else NbParam = 4; status = PCD_ProtocolSelect((NbParam+1),PCD_PROTOCOL_ISO14443A,ProtocolSelectParameters,pDataRead);... and we got a buffer overflow!
We solved the problem with :
&sharpdefine SELECT_BUFFER_SIZE 10
#nfc03a1Solved! Go to Solution.
2017-05-02 5:02 AM
Hi Samuel,
Thank you for your bug report, there is indeed a problem on the size of the buffer defined for QJE versions.
We will fix this in a future release.
Kind Regards.
2017-05-02 5:02 AM
Hi Samuel,
Thank you for your bug report, there is indeed a problem on the size of the buffer defined for QJE versions.
We will fix this in a future release.
Kind Regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.