2022-07-15 1:06 AM
Dear Sir,
When I read 2.2.4 in the datasheet, there is a Note as
Using hardware based wake-up in combination with the automatic antenna tuning feature is
not recommended. Contact your nearest ST office for further support.
Could you tell me where I can find more information about the reason?
What kind of wake-up is referred to in this note? is it the low power card detection
mentioned in capacitive sensor (4.2.4)? or Wake-up mode in 4.2.5?
Are the above functions unavailable, if automatic antenna tuning is used?
best regards
Dai
Solved! Go to Solution.
2022-07-15 5:26 AM
2022-07-15 5:26 AM
Hi,
please see AN5320 ch.6. Yes it is about 4.2.5.
BR, Ulysses
2022-07-16 7:40 PM
Dear Ulysses,
thank you very much for your advice. I read the document and got the points.
By the way, I wonder if we should use AAT function for our application. Could
you explain the typical application cases in which the AAT is necessary to
adopt for a better performance?
best regards
Dai
2022-07-18 12:12 AM
Hi Dai,
typical usage of AAT is to deal with variations, this can be manufacturing variations (e.g. part to part, board, etc), environment variations (e.g. temperature, foreign objects), coping with load from target devices, etc.
Regards, Ulysses
2022-07-18 5:54 AM
Dear Ulysses,
thank you very much for your kind explanation.
no problem about this subject.
best regards
Dai Sai
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.