2013-10-24 3:06 PM
Hello,
With L6472 I hear audible (high pitch) noise from motor when holding. volume of noise increase with increase hold current. It does not matter if the motor is loaded or not.
When I look at winding with scope one pair is the typical pwm signal locked and duty cycle appropriate for the hold setpoint
The other pair of windings appear ‘unlocked’ and much higher in frequency than the other winding.
EVAL Bd hardware
24v supply, current set point .35ampNema17, 18mh / 8.9ohms, 0.9degree step angle
Is there a setting I am overlooking
This does not occur with L6470.
thanks for your support !2013-12-16 1:14 AM
Hello,
The current control performance depends on the configuration of the parameters (off time, fast decay duration, etc). The default configuration of the IC should not be considered the one which gives best results. You could try the following configuration: Minimum on time = 3 us Minimum OFF time = 21 us tOFFfast = 10 us tSTEP = 12 us tsw = 44 us More details about the curren tcontrol algorithm are available in Kind Regards Enrico2014-05-29 9:08 AM
Dear Enrico,
I have the same problem ofthe other customer;I find thisproblemwith two different family of sanyo denki's stepper motor (you can find the datasheet in the attachment): Type 103H7126-0140 and Type 103H7123-0140;I tried
your suggested configuration but the noise still remain;
I have tryed the configuration suggested in document UM1688 pag.39/43 and the noise still remain; for testing, I'm using the evaluation board of the L6472;
I haverecorded a video that show the problem I speak; you can find the video at the following link:http://www.onetimebox.org/box/ugkLeeD3H2kgrrveg
Do you have some suggestion that can help to solve this problem? Best regards ________________ Attachments : mh7123.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzFH&d=%2Fa%2F0X0000000bIp%2F3YdOH_i_TJr9FQ0xepfMFWwJJ.mzDbiyOtTRfdo41AY&asPdf=falsemh7126.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzFC&d=%2Fa%2F0X0000000bIo%2F8hWMx2yw6PHTLXKHBxXjEzmifUCz0o8O8uFRVtS5c5k&asPdf=falseWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.