2024-01-17 7:30 AM
Hi all,
I would like to ask you about VND9012AJTR/VND9016AJTR.
1) When INPUT1 goes high (+5V) through 1k resistor, OUTPUT1 goes to +12V, OUTPUT0 goes to +2V. The same situation is with INPUT0 (=>OUTPUT0 goes to +12V, OUTPUT1 goes to +2V)
Why? I want to switch the only one channel!
2) We are switching +12V. We want to drive it with MCU with 3V3 high voltage level.
Why it is not working?
I am able to switch it on only with 5V0 high voltage level, I am using voltage generator with 1Hz frequency.
3) When I am switching both switches by only single 5V0 signal from generator, both OUTPUTs have +6V approx. Why? Switch is not digital?
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.