2023-07-24 3:38 AM
Hi,
anyone tells me how to design a 24vdc to 15vdc buck converter using viper26ld?
Solved! Go to Solution.
2023-07-24 6:29 AM
If you want to stay with STMicroelectronics, there are a bunch of devices for converting 24V to 15V, the recommendation only depends on the output current. You could e.g. have a look at theL6981 or the L6986 .
Regards /Peter
2023-07-24 4:43 AM
hi,
you have 24V IN ? and want 15v out ? then viper26 is totally wrong for this.
take a LV2862XLVDDCR or TPS563300DRLR ; which current ??
2023-07-24 6:18 AM
Thank you for your reply
Current 400mA
2023-07-24 6:29 AM
If you want to stay with STMicroelectronics, there are a bunch of devices for converting 24V to 15V, the recommendation only depends on the output current. You could e.g. have a look at theL6981 or the L6986 .
Regards /Peter
2023-07-24 6:35 AM - edited 2023-07-24 6:37 AM
or cheaper and also STM : the good old MC34063 . ->
at mouser : 511-MC34063ABD-TR
2023-07-24 6:52 AM - edited 2023-07-24 12:35 PM
The MC34063 is a very old device working with very low switching frequency, which requires bulky passive devices. In addition it is an asynchronous regulator, which requires a Schottky diode. All in all this might be the more expensive and bigger solution.
2023-07-24 9:29 PM
Thank you for your suggestion.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.