2015-02-11 1:42 PM
I'm trying to use an X-NUCLEO-IHM01A1, but without an STM32 board. That is, I need to wire up each of the necessary pins individually, sending the proper signals via another microcontroller.
For now, I just need to get to the point at which the board powers up and the green D7 LED comes on. What steps do I need to perform? I applied 3.3V to the IOREF pin on CN6 and I tied the the /RST pin on CN5 to 3.3V. Are these steps correct, and what else do I need to do?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.