2026-04-17 12:31 AM
Hello
I am currently developing an AC switch for a heating boiler in a coffee machine.
The boiler has a power rating of approx. 1200W.
To control the boiler, I have opted for a triac circuit (T1250H-6I) with an optotriac (14230634300) and ZCC. I used Application Note AN5114 to size the resistors. The description is generally excellent. However, I have a question regarding the voltage ripple on the triac. The note recommends a value of 4V. I cannot achieve this value with the standard resistor values available. My calculations give a voltage ripple of approx. 25V. Is that too much? Or what can I do to get down to the recommended value of 4V, triac with lower Igt?
Best regards
John
Solved! Go to Solution.
2026-04-20 3:07 AM
Hi Peter
Yes, you’re right. Thanks so much for your excellent help. I’ll start with this setup, build the hardware and do some tests. I can always change the components afterwards. The circuit topology is the same, anyway.
Do you have any final tips for me on triac circuits? :)
2026-04-20 5:16 AM
If you do not require the highest level of isolation with VDE0884 etc., you could also consider the STSID140-12. This thyristor and TRIAC driver has a number of advantages over classic optotriacs, including:
These bullets are explained in detail in this product presentation.
This device is the first representative of this kind; further ones with interesting parameters will follow.
There will also be an evaluation board for it soon: STEVAL-SID140V1, which also has switchable zero-crossing detection and processing, although this can only be implemented sensibly with unipolar thyristors.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.