2024-09-19 4:54 AM - last edited on 2024-09-19 5:42 AM by Peter BENSCH
Hi,
I am currently working with the VN9D5D20FN and RL78, successfully controlling 4 channels at a 100% duty cycle, achieving a 12V output. Now trying to read the current sense value for Channel 1 with OUTCFGR1 configured to 0x9FE0 and a rheostat load applied. I've readed the ADC values from the ADC1SR register and measured current consumption with a clamp meter.
Could you please assist me with the following:
Here are the ADC readings I have:
Thanks and Regards,
Vennila
Solved! Go to Solution.
2024-09-19 5:54 AM
Welcome @Vennila, to the community!
The K values are listed separately in the data sheet for the various functions in tables 57, 58, 62 and 63.
The topic of K values is also discussed in detail in AN5792. In section 2 you will find a consideration according to which your measured current of 1...2A is within a fairly large tolerance range for K.
Hope this answers your questions?
Regards
/Peter
2024-09-19 5:54 AM
Welcome @Vennila, to the community!
The K values are listed separately in the data sheet for the various functions in tables 57, 58, 62 and 63.
The topic of K values is also discussed in detail in AN5792. In section 2 you will find a consideration according to which your measured current of 1...2A is within a fairly large tolerance range for K.
Hope this answers your questions?
Regards
/Peter
2024-09-20 1:56 AM
I'm trying to find the K value. AN5792 will help me understand the K value.
Thanks for your support.
Regards
Vennila
2024-09-20 8:31 AM
in DS:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.