2006-12-21 9:33 PM
2011-05-17 1:13 AM
Hello,
As i'm using the STDV7 compiler, I would like to know the meaning of the ''missing prototype'' error. thanks :)2011-05-17 1:13 AM
Hi noscreen,
the error message you got depends from the C compiler you are using, for instance COSMIC, and not from the IDE STVD7. It means that a C function you defined in a ''.c'' module does not have a correspondant function declaration (the so called 'prototype') somewhere written in the program code (tipically the latter stays in a ''.h'' header file). I kindly suggest you to read further the C language manual normally given with the compiler tool (for Cosmic this is true), where a lot of examples often follow the definition of ANSI C statement. Best regards, TanioWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.