2025-05-27 4:53 PM
Our application requires charging a laptop at 65W via USBC with USB data passthrough to the laptop as well. A tablet computer is typically used to communicate with the laptop while it is charging. The roles would be aligned with the laptop acting as a device while charging. Does the STUSB4700 negotiation support data along with power delivery? If so, is this an NVM default configuration or would microprocessor intervention be required?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.