2018-02-05 1:55 AM
Hello,
I use STSW-SPIN3202 to drive our own motor, the maximum speed is about 1800RPM(12V, 40A, max speed 2400RPM), but I use other motor driver, it can drive above to 2400RPM.
When the motor's speed is above 1800RPM drived by the STSW-SPIN3202, it will stop the motor without any error message.
I want to know what can I do.
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.