2024-11-16 4:14 AM
I'm working on a low-power design and planning to use a STLQ020. The datasheet doesn't mention the need for a protection diode, nor does it mention that there is one integrated..
Is there an integrated protection diode?
Solved! Go to Solution.
2024-11-16 6:18 AM
Well, the data sheet does not mention a protection diode, but it does mention in the absolute max ratings: Voutmax = -0.3V ... Vin+0.3V. This means that with e.g. input = 0V, a possible voltage at the output must be limited to 0.3V, e.g. with a Schottky diode from Vo to Vi.
Does it answer your question?
Regards
/Peter
2024-11-16 6:18 AM
Well, the data sheet does not mention a protection diode, but it does mention in the absolute max ratings: Voutmax = -0.3V ... Vin+0.3V. This means that with e.g. input = 0V, a possible voltage at the output must be limited to 0.3V, e.g. with a Schottky diode from Vo to Vi.
Does it answer your question?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.