2020-09-09 3:34 PM
"...it works out of the box when placed on a suitable wireless power transmitter." is what it says on page 1 of the user manual. I have several Qi compatible transmitter pads, and the STEVAL-ISB68WA does not power-up with any of them. (D3 does not illuminate and no power is available at the output.)
Is there configuration required to get the STEVAL-ISB68WA to work with a standard Qi charger?
Joe
2021-01-13 6:41 AM
STEVAL-ISB68WA not working with standard Qi transmitters
I do have the same issue with the STEVAL-ISB68WA.
Could someone recommend a suitable wireless power transmitter that works with the EVAL Board?
BR Tom
2022-08-10 4:04 PM
Was there a list of compatible Qi chargers?
Hash
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.