2010-03-23 9:27 AM
Startup error for 12-pole BLDC motor using STM8-MCKIT
2011-05-17 1:20 AM
I have read App note AN1276 and the issue does appears to be in the alignment ramp and startup ramp table. How can I compute the correct parameter/table values for these functions? What other parameters must I set to get the system working?
2011-05-17 1:20 AM
Hello,
if you have Startup fail error it means that the required numbers of valid BEMF zero crossing detection have not been occurred. I suspect that you have to change the ramp-up acceleration to achieve the right control. To do this the best way is to use the STM8 MC Builder available at the following linkhttp://www.st.com/stonline/products/support/micro/files/stm8smcbuilder.zip
Another trivial issue: if themotor
have 12 poles this means 6 poles pairs? CiaoGigi
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.