2020-05-11 8:08 AM
2020-05-11 8:44 AM
In the L6470 the VREG pin is the output of internal 3 V voltage regulator (starting from the motor power supply) and provide an external logic supply that can be used to supply the VDD pin in order to make the device digital output range 3.3 V compatible.
The VDD pin voltage sets the logic output pin voltage range.
VDD is not internally connected to VREG, an external connection is always needed.
The AN4241 show the possible alternative supply scenarios:
Applying an external 3.3 V regulated to the VREG pin in order to supply all the internal logic you can avoid power dissipation of the internal 3 V voltage regulator.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.