2020-12-08 2:17 PM
I have a solar panel the generates about 5V @ 200mA, trying to use the solar panel (5V/200mA) and charge a single cell lithium battery with a capacity of 5000mA. Can the SPV1040 device handle this task? Thank you.
Solved! Go to Solution.
2023-07-05 12:02 AM
Well, your assumption is not necessarily wrong, but usually not sufficient. LiIO and LiPo require more precise regulation of the current and especially the voltage, which is why a dedicated battery charger chip is connected afterwards for this case.
Regards
/Peter
2024-08-08 5:39 AM
Do you think it would be sufficient to use the SPV1040 as the charger and then a common Li-ion protection module (for over charge, over discharge, short circuit and over current protection) to address these issues?
2024-08-14 2:00 AM
@m0ss As long as the voltage on the SPV1040 does not exceed the maximum value of 5.5V, you can safely operate Li-Ion modules with it. However, you should take a close look at the specifications - if something like this is available for the modules, most of which come from Asia.
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.