2020-12-08 2:17 PM
I have a solar panel the generates about 5V @ 200mA, trying to use the solar panel (5V/200mA) and charge a single cell lithium battery with a capacity of 5000mA. Can the SPV1040 device handle this task? Thank you.
Solved! Go to Solution.
2020-12-09 7:24 AM
Yes, you can do that. Please ensure that your solar panel does not deliver more than the maximum input voltage of the SPV1040 of 5.5 V.
One example could be the AN4050, which shows a high efficiency solar battery charger with embedded MPPT.
Good luck!
When your question is answered, please close this topic by choosing Select as Best.
/Peter
2020-12-09 7:24 AM
Yes, you can do that. Please ensure that your solar panel does not deliver more than the maximum input voltage of the SPV1040 of 5.5 V.
One example could be the AN4050, which shows a high efficiency solar battery charger with embedded MPPT.
Good luck!
When your question is answered, please close this topic by choosing Select as Best.
/Peter
2020-12-09 8:16 AM
so it needs to be combined with L6924D?
2020-12-09 8:29 AM
Well, you didn't specify the type of the battery yet. If we are talking about a single lithium cell rather than a lithium battery pack you should do it exactly that way, i.e. SPV1040 is supplying the constant voltage to the load plus a battery charger device such as the L6924D.
/Peter
2020-12-09 8:31 AM
yes, sorry, single cell Li Ion, thank you so much!
2020-12-09 12:38 PM
Page 13 of the app note you referenced shows that SPV1040 pin 3 is not connected to the inductor? doesn't it need the inductor to be in boost mode?
maybe I am missing something?
2020-12-09 11:12 PM
Well, fig. 17 shows to the solar power optimizer section only, but it also mentions the connection to the boost inductor at pin 3 (LX_1040).
/Peter
2023-01-15 10:00 AM
Hello Peter,
Please, can you explain why SPV1040T alone can't do the job for a single lithium cell?
Thanks
Julien
2023-06-27 4:54 AM - edited 2023-06-27 5:01 AM
The SPV1040T provides a fixed voltage that can be used for e.g. supercapacitors, lead-acid batteries and perhaps for simple LiFePO4 applications. LiIO or LiPo require a charge controller, which must therefore be connected externally.
Regards
/Peter
2023-07-04 1:28 PM
Thanks for your answer.
But section 6.3 and 6.4 deal with constant current and constant voltage which is what is needed for lipo charging.
Why is me interpretation wrong?
Regards
Julien
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.