2013-07-02 6:23 PM
Anyone know if it's possible to get the source code for easySPIN?
I bought the stepper motor eval board EVAL6474PD, but in order to control it the GUI, I need the IBU interface board (STEVAL-PCC009V2), which I don't have... I do have a several USB to SPI boards but not that one.Basically I'd like to see how the spi commands are generated based on the different user settings.. since it looks like some of the calculations are done on the chip and so only a high level command is sent.. while other, more advanced operations, must calculated offline by the host and passed to the chip as a series of low level commands. #easyspinWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.