2021-02-28 11:42 AM
I recently purchased the NUCLEO-F303RE and X-NUCLEO-IHM16M1 development kit.
With a 2804 Gimbal motor.
So far all the tests have gone well for me.
But my intention is to control a sensored BLDC motor.
Do you know of any sensored BLDC motor that works well with this development kit?
Thanks!
Solved! Go to Solution.
2021-03-24 12:50 PM
I have tried the following sensored BLDC motor R30BLB4L1 and it worked correctly for me.
2021-03-02 12:30 AM
Hello @JD.1720 and welcome to the ST Community.
I cannot suggest a brand but only to choose a three-phase brushless motor with compatible voltage and current for the STSPIN830 driver.
If you want to use the kit power supply the voltage ratings is reduced to 12 V (nominal value).
Otherwise you can use an external power supply with output voltage between 7 and 45 V (CN1 or Ja connectors).
Concerning the X-NUCLEO-IHM16M1 hardware settings you can refer to the user manual UM2415.
Let’s see if other Community Members can suggest you a specific motor part number that they used.
2021-03-17 12:55 PM
Thanks for help
2021-03-24 12:50 PM
I have tried the following sensored BLDC motor R30BLB4L1 and it worked correctly for me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.