Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am unable to write STGAP1AS configuration registers

I have a design that uses the STGAP1AS. 2 of the drivers are connected with a spi daisy chain. I am able to send read register commands and get expected default values, however i have been unable to write configuration values using the recommended co...

DSche by Associate II
  • 854 Views
  • 2 replies
  • 0 kudos

SPV1040 behaviour with a battery charger IC

Hello,I am wondering about the behaviour of the SPV1040 MPPT converter used with a battery charger (specifically the LTC4162-L but I think it would be similar with any battery charger IC). I need to charge a 2S Li-ion battery which is why I connected...

TBeno.1 by Associate
  • 1042 Views
  • 0 replies
  • 0 kudos

High frequency (high pitch beep) sound when start motor

Hi,I'm using STM32F303RB with ihm08m1 to drive a 36V BLDC motor. When I start motor, a high frequency sound (like a high pitch beep) is being made in the motor. The sound is a problem and very annoying, is there any way or solution to avoid this soun...

Alex Chen by Associate II
  • 4158 Views
  • 9 replies
  • 0 kudos

STC3117 system integration

Application note AN4870 (architecture overview) refers to "Charger IC" connected to microcontroller via I2C and to STC3117 via CD.Can you indicate a suitable Charger IC ? My project is a "true" capacity tester for single Li-Ion cell (18650). Do you ...

ALomb by Senior
  • 2066 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.