2014-04-15 8:57 AM
I'm using TIM1 for a 6-step motor control on a STM32F2xx. According of the table 4 in DM0004234 application note, I update OCxE and OCxNE at each commutation, to select a new step. When OCxE = 0 and OCxNE = 0, the output is disabled. In this case, the output seems to be in high impedance. I would rather have it in OFF-state (low Z). Is there a way to get this result?
Thanks for your help. Simon2014-05-05 2:23 AM
Ciao Simon,
For what I know you have to configure the GPIO in output mode and set the proper state (according your polarity) before to set again the same pin for AF. When OCxE = OCxNE = 0 the control of the pin is done back to the GPIO controller. Ciao GigiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.