2015-04-01 8:49 AM
Hi,
I
recently
bought
an evaluation board
STEVAL-IHM025V1 and I am having problems to make it work. I want to control a three phases induction motor. The board is supplied with 230VAC, and I can see the DC bus voltage equals to 325Vdc. I create 3 PWM with a DSPic33e, they are correctly shifted to control a 3 phases induction motor. After I control my device with this signals but the outputs aren't what I expected. I visualise the same signal for the three ouptuts, a sinus signal with a 150V amplitude with no shift. The pin SD is correctly control. So I don't know where is the matter, if you have any idea! Thank you. Benjamin L.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.