2015-02-06 10:36 AM
hello every body,
i generated header files using MC workbench, and then copy them into sys_drive_param folder. then when i open workspace in project folder. it contains only STM32F30x_userpoeject, but according to the um1054 mannual , there should also be STM32F30x_MCLibrary, can i compile the code without adding STM32F30x_MCLibrary, and batch build is necessary for web distribution lib.? please guide me..thanks2015-03-20 8:46 AM
Ciao
I think that is the same issue covered/7c38d537
. Ciao GigiWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.