2022-02-24 5:40 AM
3 Powersteps -> 3 steppingmotors for X, Y and Z axes, voltage mode.
Is there a way to switch cleanly between MOVE and RUN commands?
Currently, when I execute RUN command after MOVE movement, motors move too slowly. Although I change the speed (target - acceleration from 0 to 1200 RPM).
MOVE alone works fine, RUN curves without MOVE also clean.
Of course I wait for SMCMD_READY, and only then I send next command with SPI.
Solved! Go to Solution.
2022-02-28 11:09 PM
This was interface error . Problem solved
2022-02-28 11:09 PM
This was interface error . Problem solved
2022-02-28 11:46 PM
Thank you for letting us know!
However, you are also welcome to post more details about the temporary misbehaviour so that other users can avoid it. Thank you!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.