Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.
I would like to use a PWM to control motor speed in our particular design (like what is described in DT0001), but I could not find in the datasheet where a maximum PWM frequency, minimum high time, and minimum low time are specified for EN or FWD/REV...
Hi, everyone I want to know the value of R1 and R2. It is LD39050PU33R, and the fixed output is 3.3V. I didn't find them in the datasheet. Please help.Best Regards
Hi, here are the steps I conducted:Disable all unused sensors; stop all timers; stop ADC. Enter stop mode: ( HAL_PWR_EnterSTOPMode(PWR_LOWPOWERREGULATOR_ON, PWR_STOPENTRY_WFI);Use LPTIM1 to wake up.And here are my questions:I used integrated current ...
Hello.Can this module work in configuration as typical H bridge with controlling only 2 phases for brushed dc motor? Trigerring signals for third phase would be grounded.I see that recomended input voltage is from 125V - 400 V DC. Can this modul oper...
Hello,I am using an L5987A voltage regulator to power a ublox LISA-U200 cellular module as specified in the LISA-U200 integration manual on page 23, figure 7. I have been having issues regarding high noise under load and completely incorrect voltages...
Hello all,I'm designing a custom board based on MP1 familly and I'm using the STPMIC1APQR PMIC. To validate my design, I would like to simulate it. Is there any SPICE (Or IBIS etc) model of the PMIC available that can allow me to progress on that po...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.