2013-08-22 2:10 AM
Hi
I am a PMSM FOC v3.2 user. How can i output tacho pulse which its frequency is propotional with rotor speed. MCU is STM32F103CB in senserless Cordic. Thanks in advance.2013-08-26 5:33 AM
Ciao,
can you explain better your request? What do you mean with the following question? How can I output tacho pulse which its frequency is propotional with rotor speed.Ciao Gigi
2013-08-30 7:04 AM
Hi Gigi
it mean STM32 generates the pulse train which its frequency is propotional with rotor speed. for example; current rotor speed is 1,500RPM. And STM32 will generate pulse train which its frequency is 100Hz. (4 pole pairs) also 110Hz at 1,650RPM This is a feature of Tacho Gen. ThanksWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.