2025-08-12 4:29 AM
Hi,
I'm working with this VNQ7E100AJTR IC , I have a connected the solenoid of rating 2.2A rating at one output channel. the particular output pin got damaged and irrespective of the input the particular output pin is always High (12V). what is the maximum output current of the IC at each output channel? what the recommended output current maximum to be connected at the Output(OUTPUT0)?
1.I wanted to know whether this IC will work if PWM input is given at the INPUT0-3 in VNQ7E100AJTR IC and will the Output of this IC will be PWM or not ?
2. what is the max output current of this IC for each output Pin (4 channel).Is the output current of each channel 2A or less?
3.For OFF-state open-load with external circuitry,
4.For RPU , the value of IL(off2)min @ 4V is 3uA ?
Kindly do the needful as soon as possible
Regards.
2025-08-18 2:06 AM
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.