2019-10-21 8:00 AM
I had a problem with this component VNH5050A and I need your support.ᅠ
My test bench is composed by:
I had this problem with two different DC Brushed Motors (motor A: max operate at 16V, 5 A; motor B: works max 16V, 20A) without load.
The configuration of VNH5050 is: PWM [0-5]V, INA connect to 5 V, INB connect to GND, ENA_DIAGA and ENB_DIAGB pull-up with 3.3 kOhm to 5V.ᅠ
I read from datasheet that I could work up to 20 kHz PWM Frequency but when I reach 5 kHz of PWM Frequency I see on oscilloscope the output does not follow the input PWM signal. The output jumps some PWMs input, for more details I attach the images of the oscilloscope for the two motor.ᅠ
Legend of oscilloscope's signals: Channel 1 (yellow) VoutB (voltage between outB and GND), Channel 2 (green) PWM input, Channel 3 (blue) VoutA (voltage between outA and GND), Channel 4 (pink) Current sense pin after filter (copy from datasheet).ᅠ
I also try the configuration with 1kHz of PWM and I see the correct behaviour of the component. I attach the image for clarity, the signals of oscilloscope are the same of previous attempt.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.