2017-06-24 1:25 PM
I'm using the SPIN3201 eval board and have had it working in sensor-less and Hall modes, but i'm looking for better low very low speed, < 10 rpm behaviour where the halls don't produce smooth torque.
I've attached a 1000 pulse quadrature encoder and from the monitor in ST Motor Control i can see RPM when i turn the motor by hand so i believe it correctly connect or it wouldn't report motion. However, i cant get the motor to move, the alignment step doesn't seem to do anything, as i understand it should drive one coil to pull the motor to a known position, but it doesn't, though it reports success in the ST Motor Control Monitor. Then when i try and start the motor i get nothing, no moment, no sounds, no volts on the terminals also no error.
Any one got any hints what i'm doing wrong?
Thanks
Tim
2017-12-14 11:40 AM
Hello, I have the same problem, exactly how you described. Did you solve the problem?
Thanks
Francisco
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.