2025-01-30 8:22 AM - last edited on 2025-01-30 12:00 PM by Peter BENSCH
Hello Team
I am looking at how i can buy the reference for evaluation board STEVAL-ISV002V1
or the and the gerber files if possible.
any assistance would be appreciated.
regards
joshua
Solved! Go to Solution.
2025-01-31 1:13 AM - edited 2025-01-31 1:15 AM
Ah, now everything is clear. The STEVAL-ISV002V1 is indeed obsolete, which is why there is no documentation for it from ST. Actually, this also includes the AN3095, which should therefore no longer be visible either. If you can't find it somewhere in the depths of the never-forgetting internet, nobody can help you.
Sorry I can't give a more pleasant answer.
Regards
/Peter
2025-01-30 9:00 AM
Did you check the 'CAD Resources' tab on the Product Page:
https://www.st.com/en/evaluation-tools/stdes-isv002v1.html#cad-resources
2025-01-30 9:12 AM
Hi Andrew
Thanks for that i actually didnt see that section.
however i am still not able to find it there as the board status says obsolete is it possible that this is the reason i dont see any CAD resources ? .
otherwise i didnt see that section.
regards
josh.
2025-01-30 11:57 AM
When I open the website, nowhere do I find that it is obsolete - where did you see that?
The fact is, however, that all boards whose designation begins with STDES are only design studies of the respective product division and cannot be purchased. However, you can download all the data from the CAD Resources tab (here BOM, schematics, ORCAD Design Files and Board Holder, reachable from the URL @Andrew Neil mentioned before), and use it to build your own board.
Regards
/Peter
2025-01-31 12:06 AM
Hello Peter
Thanks for the response , Sorry for the confusion the board i am looking for is not starting with STDES
it is STEVAL-ISV002V1 Application note AN3095
Full file name .
STEVAL-ISV002V1 3 kW grid-connected PV system,
based on the STM32x
link
STEVAL-ISV002V1, STEVAL-ISV002V2 3 kW grid-connected PV system, based on the STM32F103xx
Looking forward to your advise .
regards
josh.
2025-01-31 12:17 AM
@JoshuaNgalande wrote:the board i am looking for is not starting with STDES
Apologies - I put "STEVAL-ISV002V1" into Google, and it gave me "STDES-ISV002V1"
2025-01-31 1:13 AM - edited 2025-01-31 1:15 AM
Ah, now everything is clear. The STEVAL-ISV002V1 is indeed obsolete, which is why there is no documentation for it from ST. Actually, this also includes the AN3095, which should therefore no longer be visible either. If you can't find it somewhere in the depths of the never-forgetting internet, nobody can help you.
Sorry I can't give a more pleasant answer.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.