2025-03-28 3:58 AM
We have implemented the following circuit. This matches the application circuit given in datasheet of LDO29300P2MTR.But it does not yield expected output. We need help!!
Solved! Go to Solution.
2025-03-28 9:57 PM
The chip gives expected output 12V but within a fraction of second , voltage drops to 0V.
2025-03-29 4:25 AM
Thanks for the help. LD29300P2MTR will work on 2.5 V to 14V only. it will never work greater than 14V. We can use the MIC29302WU
Thanks &Regards,
Saravanan G
2025-03-29 12:55 PM
Sorry, I had also overlooked this during a cursory glance at the data sheet: although the LD29300 can withstand an input voltage of up to 30V, it actually only works up to 14V. This can be found in the data sheet as footnote 1 under table 2:
Above 14 V the device is automatically in shutdown.
Regards
/Peter
2025-03-31 1:42 AM
@Peter BENSCH wrote:This can be found in the data sheet as footnote 1 under table 2:
Above 14 V the device is automatically in shutdown.
So it does!
@saran - here:
@saran - always important to understand that these "Absolute Maximum" ratings are not operating specs!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.