2013-09-12 5:43 AM
Hello,
I don't know if this was the subforum for this chip, but here's my problem:In the datasheet of the L6360 you show that the microcontroller and the L6360 are connected through UART (USART).But how do you configure, read or write through the UART?There are no commands nor any hints given.Also the IO-spec states that the IO-Link chips can be programmed (IODD, user program), but there are no pins for that?I hope to hear from you soon. #l6360-io-link #l6360-io-link2013-09-16 7:49 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.