2019-02-07 8:37 AM
Hi everyone. I'm working on to drive 3 wheel omniwheel system for our project. I'm using parallel connection to have larger current. I realize that when i connect all the input and enable pins to ground (logic 0), all the leds connected to the outputs of the H bridge are slightly ON. My question is why does all outputs start as HIGH state during when all inputs are in LOW state. I only supply 12 volts to the power input.
Thank you for your answers.
2019-02-18 1:51 AM
When the EN is low the power outputs are floating. I suppose there is nome leakage strong enough to slightly turning on the LEDs.
2019-02-25 10:06 AM
Thanks for your answer Mr. Poli . It is probably leakage current because they are not seen as fully ON state.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.