2017-10-20 5:16 AM
Hi,
I'm repairing an audio power amplifiers from a top model manufacturer like Harman-Kardon, Dynaudio, Bose from cars. And in almost all of models I faceing up with broken regulator L5973. The failure is that the voltage on the output increases to 4-5V causing a damage in connected DSP chips. This is standard application from page 9 from the ST datasheet. Input is 12V output is 3,3V.
What can be a root cause of this behaviour? When I replace for new IC it is working in next coulpe of months ok and again fails.
Maybe somebody had this case and could share some ideas
Regards,
Pawel
2025-03-15 8:25 AM
Hello, i am repairing a harman kardon with the same IC L5973scheme, i have one for 3,3V and another with 1,2V. The first step (3,3V) is damaged, measuring 4,9V.
I think the problem is age and moisture...
You only replace that IC or broken any more?
Thanks in advance
2025-03-15 10:10 AM
L5973 has a max input voltage of 36V, so a strong spike can cause degradation over time.
Check with an oscilloscope if voltage spikes are exceeding 36V.
Use a TVS diode (like SM8S36A or SM8S33A) on the 12V input to clamp spikes.
Add a low-ESR bulk capacitor (1000µF, 25V or higher) to absorb transients.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.