2025-12-02 9:12 AM - edited 2025-12-02 9:12 AM
Hi,
We wish to do a Boost PFC with L4986A and a 30uH inductor.
Power is 2200W and Mains is 85-265VAC.
When the mains is at 240VAC, the inductor current would be discontinuous for some 80% of the mains half cycle.
Is this OK?
Will the L4986A be able to control it to give a good power Factor with low THD?
Solved! Go to Solution.
2026-03-05 11:07 AM
If the question is still relevant:
the L4986A is designed for continuous‑conduction‑mode (CCM) boost PFC. At 240VAC and 2.2kW with only 30µH, operating 80% of the half‑cycle in discontinuous mode is not the intended use case.
In deep DCM the current waveform and loop gain change significantly; you can still get PFC action, but PF and THD will generally be worse and not in line with the datasheet performance figures.
For good PF/low THD you should:
So with 30µH at 2.2kW I would not expect optimal PF/THD with L4986A.
Hope that helps?
Regards
/Peter
2026-03-05 11:07 AM
If the question is still relevant:
the L4986A is designed for continuous‑conduction‑mode (CCM) boost PFC. At 240VAC and 2.2kW with only 30µH, operating 80% of the half‑cycle in discontinuous mode is not the intended use case.
In deep DCM the current waveform and loop gain change significantly; you can still get PFC action, but PF and THD will generally be worse and not in line with the datasheet performance figures.
For good PF/low THD you should:
So with 30µH at 2.2kW I would not expect optimal PF/THD with L4986A.
Hope that helps?
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.