2019-10-14 5:59 AM
Dear all, we are using the STPM32, and we calibrate it with a 50Hz load. In some cases, customers need to use it at 60Hz. Is the accuracy obtained from the calibration still valid? On documents, I can't find this in formation.The only statement is: "Setting the default line frequency through REF_FREQ bit in register DSP_CR3 speeds up the period calculation algorithm convergence". We can change this bit with firmware, but I wonder if the accuracy doe'snt change. Thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.