cancel
Showing results for 
Search instead for 
Did you mean: 

ISO808 reverse protection and maximum current. 2nd question Are the 0.01uF necessary?

SPave.1
Associate

Good Morning/Afternoon.

 

Thanks for your time.

I must use 2 ISO808TR in a project.

Because of the large current requested (0.5 A * 8 *2 = 8 A or worse 0.7A *8 *2 = 11.2A) and the absence of heat dissipator (orange derating curve) I could not use a diode as reverse voltage protection. 

SPave1_0-1687419281234.png

Because of lack of time I could not use (because I could not test before the final product) a solution control + MOS based like LM5050-1 or similar.

So I need to ask about reverse protection of ISO808.

In page 24 (Chapter 8) of https://www.st.com/resource/en/datasheet/iso808.pdf it is not said if Is of the diode is Icc of Table 4 (from 5.5mA to 16mA). I think that in reverse polarity protection the diode should be off and the only current is the irrilevant reverse current.

From the following note I assume that it is; so I only need a signal diode and not a power diode

"In normal operation (no reverse polarity), there is a voltage drop (ΔV) between GND of the device and GND of
the system. Using option 1, ΔV = Rgnd * Icc. Using option 2, ΔV = VF@(IF)."

 

SPave1_3-1687420109508.png

My question is with the following values

  • VCC = 24 -30 V
  • and Rgnd = 10K Ohm (=> 30V*30V/10K = 0.09W; a normal 0805 resistor will work; 30V/10K = 3mA << 25 mA) 
  • and VSSA310SHM3_A/H  (Vrrm =100V)  diode (If = 3A >> 16 mA) . 

Should I expect any problem?

-----------------------------------------------------

2nd question

Are the 0.01uF used in development kit strictly necessary and where should be placed?

Are they forced to be on the same plane (top or bottom) of ISO808?

There is no gerber, only schematics.

 

SPave1_4-1687420860221.png

Thanks for your time.

Best Regards

 

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.