2020-02-13 10:19 PM
I want to control position using STEVE-SPIN3204.
BLDC 24V motor and external encoder were used and it was set as position controller. I compiled and downloaded it, and when I start the motor, the motor vibrates.The way I know 1) motor start 2) Move the purpose positionIt is.The motor vibrates and the operation does not work at all.Is there a way?
2020-02-13 10:21 PM
It's STEVAL-SPIN3204.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.