2021-06-23 6:45 AM
Model: STBB2J30-R
The circuit is the same as "Figure 1. Application schematic for fixed version" on page 3 of the data sheet.
However, the output voltage is 2.8V instead of 3.3V.
Is there a similar event? If so, please tell me the details.
The settings are as follows.
VIN: 4.6V
EN: connected to VIN
BP: 0
MODE: 0
VSEL: connected to VIN
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.