2019-10-16 4:40 AM
Hi All,
I'm working on a project (Street Lamp), wherein we required some metering parameters. So, I've brought an EVALSTPM34 board for speeding up the development process. On the "STPM3x Evaluation software" I was able to read all the necessary parameters ( except Line frequency and Power Factor). I could not able to find the registers these two parameters.
In addition to that, later, I'll interface the EVALSTPM34 with my STM32F09x controller. Hence, I wanted to know the UART commands and their sequence as well.
At the moment, our production line is in the halt state. Therefore, any support or help would be highly appreciated.
The parameters which I required are listed below:
Regards,
Aatif Shaikh
@Community member
@Claire OKU
@brk
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.