2019-06-04 10:42 AM
I am using an L6599A high voltage resonant controller in my AC/DC power supply, and I want to add a shutdown feature. I have pulled the STBY pin to GND of the chip, however the output continues to produce pulses.
Latching shutdown (via DIS pin) is not what I want, so is there any other way to stop output pulses without removing AC power from my system?
NOTE: This question and answer originated from a customer support case which was handled by us. We regularly review support cases and add any helpful ones here for all to benefit from.
Solved! Go to Solution.
2019-06-04 10:43 AM
There are two ways how to achieve the desired function:
1. The VCC pin can be pulled below VCC_OFF threshold (7.45V). See Table 5 “Electrical Characteristics�? of datasheet for more information.
2. The LINE pin can be pulled below 1.24V. See chapter 7.6 “Line sensing function�? of datasheet for more information.
2019-06-04 10:43 AM
There are two ways how to achieve the desired function:
1. The VCC pin can be pulled below VCC_OFF threshold (7.45V). See Table 5 “Electrical Characteristics�? of datasheet for more information.
2. The LINE pin can be pulled below 1.24V. See chapter 7.6 “Line sensing function�? of datasheet for more information.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.