Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ATEAVAL-IPFC01P1 abnormal operation phenomenon

HelloI have ATEAVAL-IPFC01P1 and I have two questions during the test of operation.If the load is not applied, it operates normally,however, PWM1 and PWM2 signals are not output when load is applied.As a result of checking the signals of STEVAL-IPFC0...

Kdaeg.6 by Associate
  • 692 Views
  • 0 replies
  • 0 kudos

About L6201P 's Cooling heat sink!

I want use L6201PS for my BDC motor. there is a heat pad under the chip. Should I connect the Head pad to the GND? Or just leave it floating net ? Thanks!

Ztao by Associate
  • 790 Views
  • 0 replies
  • 0 kudos

+3.3V, 0.6A using STEVAL-ISA136V1

Hi,We are using STEVAL-ISA136V1 for our application. We need +3.3V, 0.6A output instead of +5V, 0.6A as per STEVAL-ISA136V1. Let me know what value changes in feedback resistors are required or if any other changes are requiredRegards,Kamesh Lakhwani

KLakh by Associate II
  • 676 Views
  • 0 replies
  • 0 kudos

+15V, 1A using STEVAL-ISA140V1

Hi,We are using STEVAL-ISA140V1 for our application. We need +15V, 1A output instead of +12V, 1.25A as per STEVAL-ISA140V1. Let me know what value changes in feedback resistors are required or if any other changes are requiredRegards,Kamesh Lakhwani

KLakh by Associate II
  • 506 Views
  • 0 replies
  • 0 kudos

EVLSTNRG - 1KW Product Inquiries

HiI would like to make battery charger by applying EVLSTNRG-1KW  ** BATTERY CHARGER SPECIFICATIONSTotal capacity – 3 [KW]input voltage – 100 ~ 420 [VDC] (input from solar panel)3. output voltage – max 430 [VDC] (battery charger voltage)  ** Question1...

KYOON by Associate
  • 1066 Views
  • 1 replies
  • 0 kudos

l6566bh-based smps design is failed to start up

we have designed a wide range FlyBack SMPS (200VAC-->420V AC Input) multiple output (26V 4A)but our system couldnt start up and ıt stuck to burst mode despite of havıing 0,5A ldummy load alwasys connected to the output of the smps.the Vgs signal (pu...

AZ by Associate
  • 996 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.